text.skipToContent text.skipToNavigation

Cold & Flu Prevention Supplies

Help Protect Your Employees During this Cold & Flu Season


 


According to the Centers for Disease Control and Prevention (CDC)...

Preventative Steps

• Try to avoid close contact with sick people.

• While sick, limit contact with others as much as possible to keep from infecting them.

• If you are sick with flu-like illness, CDC recommends that you stay home for at least 24 hours after your fever is gone except to get medical care or for other necessities. (Your fever should be gone for 24 hours without the use of a fever-reducing medicine.)

• Cover your nose and mouth with a tissue when you cough or sneeze. After using a tissue, throw it in the trash and wash your hands

• Wash your hands often with soap and water. If soap and water are not available, use an alcohol-based hand rub.

• Avoid touching your eyes, nose and mouth. Germs spread this way.

• Clean and disinfect surfaces and objects that may be contaminated with germs like flu.

For more information, visit: CDC: Preventive Steps

Cold vs. Flu

Flu and the common cold are both respiratory illnesses but they are caused by different viruses. Because these two types of illnesses have similar symptoms, it can be difficult to tell the difference between them based on symptoms alone. In general, flu is worse than the common cold, and symptoms are more intense. Colds are usually milder than flu. People with colds are more likely to have a runny or stuffy nose. Colds generally do not result in serious health problems, such as pneumonia, bacterial infections, or hospitalizations. Flu can have very serious associated complications.

Cold vs. Flu Symptom Difference

The symptoms of flu can include fever or feeling feverish/chills, cough, sore throat, runny or stuffy nose, muscle or body aches, headaches and fatigue (tiredness). Cold symptoms are usually milder than the symptoms of flu. People with colds are more likely to have a runny or stuffy nose. Colds generally do not result in serious health problems.






For more information, visit: CDC: Cold Versus Flu