text.skipToContent text.skipToNavigation

SUCCESS STORY: ELIMINATED SLIPPAGE ALSO MEANS ELIMINATED DOWNTIME


Continental Synchrochain Carbon for the win. A large food industry customer was experiencing v-belt slippage at the pre breaker screw conveyor drive. The system was running a multiple v-belt drive, and having any type of slippage could affect overall production.

Applied® worked locally with Continental representatives, to make recommendations and plan a more effective solution. Together, they were able to redesign the drive with Continental Synchrochain Carbon. In doing so, the new drive not only weighs less and requires less maintenance, but slippage was eliminated and production was increased. This solution will also save the plant an estimated $430 per year in energy costs.

SUCCESS STORY: BREAKING THE CHAINS OF MAINTENANCE


Continental Synchrochain Carbon comes to the rescue. A conveyor system used to transfer hay was running an 80-2 double chain. Buildup and consistent wear on the sprockets, caused by the harsh, dusty environment, meant the chain could not stay properly lubricated to function efficiently or effectively. Therefore, the sprockets and chain wore out prematurely. Seeing this as a great opportunity to provide a better solution, Applied® worked with Continental and the end user, to recommend and implement better tools to get the job done. Since utilizing Continental Synchrochain Carbon, the customer has realized a smoother run, increased uptime and a cost savings, since the conveyor has been running trouble free.

SUCCESS STORY: SYNCHRONOUS DRIVES IN SERIOUS NEED OF AN UPGRADE


A supplier was having a temperature issue with some of their drive components, and turned to Applied® for help. Applied® worked with Continental representatives to make recommendations and suggest a possible design adjustment. Together, they were able to redesign a drive for an air cooled heat exchange application, utilizing Continental Synchrochain Carbon. By doing this, the drive width was reduced by more than an inch, the drive high dropped by 72 lbs. and the overall cost was decreased by half.

WHY CONTINENTAL CONTI® SYNCHROCHAIN CARBON?

As a high horsepower capacity power transmission belt, manufactured with an extremely durable polyurethane body, and carbon tensile members, it can replace the most demanding chain drives in the same space or less.

Available Size Options

MORE REASONS WHY YOU SHOULD SWITCH TO CONTI® SYNCHROCHAIN CARBON:

SYNCHROCHAIN CARBON ADVANTAGES
  • Reduces drive width by up to 5 times
  • No lubrication needed - Operates clean and dry
  • Smooth engagement of teeth and reduced vibration
  • Quiet in operation
  • High-speed capability
  • 2-3x life expectancy
  • Length is stable through life
CHAIN DRIVE DISADVANTAGES
  • – 90% of chain drives are improperly lubricated
  • – Lubrication attracts debris causing wear problems
  • – Jerky motion causes vibration
  • – Metal-to-metal contact makes chain drives noisy
  • – Limited speed range
  • – Limited life
  • – Wear and elongation

WHERE CONTI® SYNCHROCHAIN CARBON CAN REDUCE COSTS:

  • Conveyor Systems
  • Bucket Elevators
  • Overhead Hoists
  • Food Processing
  • Warehouses
  • Foundries
  • Sand & Gravel Plants
  • Packaging Machines
  • Pumping Stations
  • Extrusion Presses
  • Spindle Drives
  • Feed Drives
  • Wire Drawing
  • Saw Mills
  • Injection Molding Machines

Benefits & Features

Can be an ideal replacement for problem v-belt drives, and can also replace standard rubber timing belt drives, but in a much narrower drive envelope. Provides the end user with smooth, energy efficiency, high capacity and dramatically improved up-time.

Features

  • Nearly maintenance free
  • Higher power capacity
  • Longer service life
  • Wear-resistant
  • Abrasion-resistant


DISCLAIMER: The above content is provided by the supplier. Applied does not guarantee the accuracy or timeliness of the content. The above content is provided “AS IS”,
AND ANY AND ALL EXPRESS AND IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS ARE HEREBY EXCLUDED. All warranties, if any, are solely from the supplier.