Skip to content Skip to navigation menu

GEARWRENCH Mobile Work Station:
Purpose Built & Ready to Roll


With so many features, the GEARWRENCH Mobile Work Station is more than just a tool chest on wheels. It’s built with industrial and automotive jobs in mind, keeping tools and supplies organized, while housing more combined drawer, locker, and tray volume than the closest competitor in the strongest frame in the business. Applied Industrial Technologies is excited to offer GEARWRENCH Mobile Work Station.

We start with the strongest frame in the business because we know this beast is going to need to hold a lot. Like 19,000 cubic inches of combined drawer, locker, and tray volume – nearly 20% more than the closest competitor. The Mobile Work Station has a total load capacity of one ton and each of its 11 ball bearing slide drawers is rated at 100 pounds. It rolls easily on bigger, tougher wheels than any of the other guys – each of its 6x2-inch industrial grade polyurethane locking casters has a capacity of 800 lbs. With Mobile Work Station extras like vise-mount capability, locking storage, a built-in 6-outlet, 2 USB port power strip, and more, we’ve once again raised the bar on productivity innovation.

WHY GEARWRENCH MOBILE WORK STATIONS?

With a total load capacity of one ton - each of its 11 ball bearing slide drawers is rated at 100 pounds, and locking drawer pulls for safety, the GEARWRENCH Mobile Work Stations are ideal to use in your toughest and roughest work environments.

Available Size Options

Features & Benefits:


• 19,000 cubic inches of combined drawer, locker, and tray volume – nearly 20% more than the closest competitor

• EVA drawer liners and top mat

· Pegboard surface and side/back hooks for added storage capacity

• The lockable side cabinet is separate from the main unit's drawers

· Rolls easily on bigger, tougher wheels than any of the competition – each of its 6x2 inch industrial grade polyurethane dual-locking casters (2 swivel, 2 rigid) has an 800 lb. capacity

• Innovative design features: vise-mount capability, locking storage, and a built-in 6-outlet, 2 USB port power strip

· Heavy-duty 20 gauge steel frame - the industry’s strongest

• Achieving a new standard in mobile work stations


DISCLAIMER: The above content is provided by the supplier. Applied® does not guarantee the accuracy or timeliness of the content. 
The above content is provided “AS IS”, AND ANY AND ALL EXPRESS AND IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS ARE HEREBY EXCLUDED.
All warranties, if any, are solely from the supplier.