Skip to content Skip to navigation menu
01_Landing Page Hero_NSK Reconditioning_700x400.png

Revitalize Your Bearings with NSK's Comprehensive Reconditioning Program


WHAT IS RECONDITIONING?

Reconditioning brings used bearings back to life. This is accomplished through various procedures that may include: cleaning, polishing, grinding, replacement, resetting and refinishing. This process restores bearings, bringing them back to like-new specifications and performance.

WHEN TO RECONDITION?

Routine maintenance checks can indicate signs of bearing fatigue and a need for further inspection. In addition, knowing the history, performance and operating environment will provide indications as to the condition of the bearing. Not all bearings will benefit from reconditioning. Some bearings may be too damaged, requiring the purchase of a new bearing. NSK can help you determine whether reconditioning would be beneficial for your specific bearing requirements.

WHY RECONDITION?

Many times, a bearing can be reconditioned and placed back into service, extending the life of the bearing while avoiding the possible high cost and lengthy lead times of a new bearing. Reconditioned bearings that are not returned to service immediately, but stored for later service, can reduce inventory costs. Reconditioning can cost a fraction of the time and money compared to new. Original specifications are used to ensure the bearing’s quality, functionality and performance. A warranty is provided to further support the quality of work used to recondition the bearing. Reconditioning is a timely, reliable and cost-effective means of maintaining productivity and reducing downtime.

WHO TO TRUST?

NSK strives to provide their customers with the best options available to keep their businesses running smoothly. The reconditioning program is not limited to NSK branded bearings. They welcome various brands, types and sizes of bearings. Their reconditioning lead times are among the shortest in the industry based on industry standards and given the reconditioning level required. They want customers to continue their success. NSK’s reconditioning reports include a thorough damage analysis to help customers assess the cause of the problem, enabling them to prevent issues that would reduce the life of the bearing in the future.

NSK offers bearing reconditioning in four different levels:

 

LEVEL R4


• Pressure cleaned
• Inspected with thorough damage analysis
• Raceway, bore, cup, cone, inner, outer & roller angles verified
• New components (rollers or rolling elements, pins & cage rings) if applicable
• Raceways reground as needed
• Polished, vibratory finished/touched up as required
• Verified for size & angle
• Clearances measured, verified & reset
• Cleaned & repacked

LEVEL R3


• Pressure cleaned
• Inspected with thorough damage analysis
• Raceway, bore, cup, cone, inner, outer & roller angles verified
• Raceways reground as needed
• Polished, vibratory finished/touched up as required
• Verified for size & angle
• Clearances measured, verified & reset
• Cleaned & repacked

LEVEL R2


• Pressure cleaned
• Inspected with thorough damage analysis
• Polished
• Minor repair (spalls/imperfections)
• Measured and spacers reground if applicable
• Proper clearances checked
• Cleaned & repacked

LEVEL R1


• Pressure cleaned
• Repackaged

02_Landing Page Hero_NSK Reconditioning_700x400.png

Ready to get started?


The reconditioning process begins by simply contacting your Applied representative about your bearing needs!

They will work with you in coordinating with NSK’s reconditioning facility to inspect the damaged bearing and provide a quotation and inspection report specific to the bearing(s) requiring reconditioning. Upon receiving your authorization, the damaged bearing will undergo the appropriate reconditioning processes.

The reconditioned bearing will be securely repackaged and delivered to you within the quoted lead time. If the quotation is declined, Applied and NSK will make arrangements to dispose of, or return your damaged bearing.


DISCLAIMER: The above content is provided by the supplier. Applied® does not guarantee the accuracy or timeliness of the content. 
The above content is provided “AS IS”, AND ANY AND ALL EXPRESS AND IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS ARE HEREBY EXCLUDED.
All warranties, if any, are solely from the supplier.