Skip to content Skip to navigation menu
01_Banner_Industry Web_1284x175_Longer FADE.png

PPI Sanitary Components - Food Grade


The food industry has exceptionally high standards. If products fail to meet these standards, the impact could be significant. This is why so many in the industry trust PPI for their sanitary conveyor component needs. With over forty years of experience in the industry and the invaluable knowledge gained from their food division companies, KOFAB® and Meyer® Industries, Inc., customers can have confidence that they understand the challenges of the industry and how to overcome them.

K-Drive


PPI’s K-Drive is an engineered, one-piece pulley that drives today’s newest technologies of positive drive, low to no tension conveyor belting for the food industry.

This patented design combines composite and stainless steel to create one of the most sanitary designs for positive drive conveyor belting in the industry.

The K-Drive can be built to accommodate different styles of positive drive conveyor belting. As a drop in replacement of square shaft and sprockets assemblies, it will make your conveyor even more hygienic.

K-DRIVE REPLACES THE SHAFT AND SPROCKET DRIVE FOR A MORE SANITARY, EASY-TO-CLEAN OPTION.

Existing assembly drives consists of a square shaft with locking collars or snap rings to position sprockets in place.

These assemblies are difficult to clean and lends themselves to migrating sprockets which decreases drive efficiency.

PPI’s revolutionary one-piece, K-Drive technology eliminates those components for ease of cleaning and provides superior wear and less belt stress.

K-DRIVE REVOLUTIONARY DESIGN

• Eliminates the need for shaft collars and snap rings

• Eliminates chances of sprockets breaking infield

• Greater sanitation due to few parts and press-fit shaft design

• Superior pulley and belt wear due to use of acetal

FEATURES & BENEFITS:

• Positive drive system

• Self-tracking belt

• Sanitary design

• Low-maintenance

• Quiet operation

• Various design options

KV Drive


PPI has designed and engineered a pulley product that will eliminate slipping, belt tracking and sanitation concerns. The patented KV Drive Pulley has a positive, quiet and self-tracking feature with 304 stainless steel construction and 3-A dairy approval. The composite and stainless steel option has FDA approval and is extremely sanitary. Originally designed to drive the Volta SuperDrive™ belt, it can be used to run on other belts such as the flat belt and standard “A” section V-Guide belt designs. The KV Drive Pulley, when used with the Volta SuperDrive belt, will outlast and outperform modular belts with plastic sprockets.

FEATURES & BENEFITS:

• Positive drive system

• Self-tracking belt

• Sanitary design

• Low-maintenance

• Quiet operation

• Various design options

• Available in multiple material options


DISCLAIMER: The above content is provided by the supplier. Applied® does not guarantee the accuracy or timeliness of the content. 
The above content is provided “AS IS”, AND ANY AND ALL EXPRESS AND IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS ARE HEREBY EXCLUDED.
All warranties, if any, are solely from the supplier.