Skip to content Skip to navigation menu
Leeson_articlelogo.png

Success Story: Reducing Food Processing Plants' Operating Costs


A major food supplier was experiencing issues pertaining to motor failure, to the tune of failure over 200 times per year. Such outages cost hundreds of dollars per minute in downtime! Conveyor belts with standard motors couldn't hold up to the wear and tear of production, exposure to chemicals and high pressure from washdown. Other motors were swapped in, but to no avail.

This organization turned to Applied® in partnership with Leeson, to develop the Leeson 2 HP Extreme Duck encapsulated, stainless steel motor. The first variation was installed to see if it would work, and what type of difference it could make. Within one year of being installed on the conveyor belting, the motors only needed to be switched out 250 times. This was a stark improvement, but still left room for progress.

Within the next two years, the motor experienced enhanced redesign. The result is the Extreme Duck Ultra Motor - which lacks crevices to house bacteria, is steam- and waterproof, and contains a "Totally Enclosed, Not Ventilated" (TENV) design. This motor is now certified as IP69k, confirming its design as impenetrable to dust and liquids, in any mounting position, and non-wicking lead wires, that are colored and numbered for proper identification during the installation period.

Why Leeson Motors?

Leeson premium efficient motors are totally enclosed and boast NEMA-exceeded efficient ratings. These washguard industrial-duty motors are tough enough to handle exposure to water, dust and corrosives all day, every day.

Available Size Options

Washdown Motor Selection Guide

Download Pdf