Skip to content Skip to navigation menu
04_Banner_Industry Web_1284x175_Longer FADE.png

SealMaster_articlelogo.png

Original Sealmaster® Paver Bearings from Regal - Aggregate


 

The Sealmaster® brand of bearings has always been synonymous with quality, problem solving and performance. Those same attributes also hold true for Sealmaster paver bearings.

As a well-known and well-respected name in the paving industry, Sealmaster has maintained close partnerships with paver original equipment manufacturers. Their team of engineers have worked with these manufacturers to design bearings that can endure the harsh environments of the paving industry.

As asphalt paving technology has evolved, so have the performance requirements of paving equipment. Sealmaster has and will continue to incorporate the most innovative materials and technologies into our paver bearings.

Once available only to the manufacturers of paving equipment, Sealmaster brand paver bearings are now sold by Applied®, making the bearings more available than ever.

The Sealmaster® Difference:


SEALMASTER® Paver Bearings Nomenclature:


Features & Benefits:

  • High Temperature Contact Seal - The double lip high temperature contact seal is the most popular design used
  • Nomex* Seal with Flinger The Nomex seal provides a high temperature - tight labyrinth seal which retains lubrication and acts as a filter to exclude contamination
  • Ductile Iron End Cap A tough - wear resistant end cap that helps keep asphalt from forcing its way into the bearing
  • Rotating Shield - The black oxided shield is fixed to the extended inner ring and precision machined to run with a small clearance with the end cap
  • Self-Adjusting Washer A conical-shaped mechanical seal is located directly behind the rotating shield supplying the bearing with a third contamination barrier

DISCLAIMER: The above content is provided by the supplier. Applied® does not guarantee the accuracy or timeliness of the content. 
The above content is provided “AS IS”, AND ANY AND ALL EXPRESS AND IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS ARE HEREBY EXCLUDED.
All warranties, if any, are solely from the supplier.