Skip to content Skip to navigation menu
03_Landing Page Hero_SKF Cooper_700x400.png

SKF COOPER BEARINGS: HIGH QUALITY. LOW DOWNTIME.


Don’t let worn or subpar bearings slow down your operations. SKF Cooper Bearings offer a high quality and wide range of split-to-the-shaft bearings, when compared to others available on the market. Designed with simplicity in mind, these bearings can be fitted, removed and inspected without having to dismantle surrounding equipment, resulting in less time for installation, changeover and inspection.

SKF Cooper's split-to-the-shaft cylindrical and double row tapered roller bearings deliver cost savings by supplying high quality bearings that help reduce downtime and increase uptime -- ideal for countless applications, even in the most challenging environments.

According to SKF, their Split-to-the-Shaft Bearings disassemble into smaller components easing the task of lifting and handling, and also making assembly or changeout simple, even in the most cramped and inaccessible conditions. Clearances are pre-set, so no on-site adjustment is needed and no specialist fitting tools are required.

SUCCESS STORY: STEEL MILL SAVES TIME, MONEY, WEAR AND TEAR


The Babbitt bearings in a steel mill’s four baghouse fans needed constant lubrication, which made reservoir refills and proper cleanup part of the mill’s daily routine. Overtime, this cost time and money for the facility.

Since the eight bearings in place lasted just three to four years each, one needed to be changed out about every six months; additionally, bearing failures often caused shaft damage.

A change to grease-lubricated SKF Cooper Split-to-the-Shaft Bearings eliminated the housekeeping challenges, and corresponding shaft damage, with a projected annual savings of $12,000 in oil and routine maintenance alone. It is expected that not only will the mill save in oil and maintenance, but according to SKF, the life of their Cooper bearings is at least 180,000 hours, or 2-to-4 times longer, than that of previous bearings.

SUCCESS STORY: Solid Bearing Failure Turns into An Applied® & SKF Success


A major automotive OEM was faced with the failure of a solid bearing in an SAF pillow block, which threatened to cost $24,000 in repairs, plus a five-day shutdown of the assembly line. To fix, crews would have needed to completely remove the main conveyor shaft to disassemble bearings and sprockets, disconnect the vehicle transfer chain and steel I-beams, just to allow clearance for the removal. Not only could this method prove to be incredibly labor intensive, it could also have contributed to the disruption of other parts and their functionality.

By utilizing an SKF Cooper Split-to-the-Shaft Bearing as a replacement for the solid bearing, easier installation without disassembling the shaft or chain was possible.

It is estimated that this saved over 400 hours and at least four days of downtime, not to mention, the SKF Cooper bearing is expected to have an overall longer service life.

WHY SPLIT-TO-THE-SHAFT ROLLER BEARINGS FROM SKF COOPER?

With an aluminum Triple Labyrinth seal to ensure a superior seal, a cartridge and pedestal’s spherical design to compensate for misalignment, and inner race clamps to improve shaft protection, this should be the only roller bearing you reach for.

Available Size Options

MEET SOME OF YOUR MOST COMMON APPLICATION REQUIREMENTS, WITH THESE POSSIBLE MOUNTING OPTIONS:


MORE REASONS YOU SHOULD SWITCH TO SKF COOPER SPLIT-TO-THE-SHAFT ROLLER BEARINGS:

COMMON INDUSTRIES:
  • Designed to reduce:
    – Installation
    – Changeover
    – Inspection time
  • Superior seals
  • Compensation for misalignment
  • Shaft protection
  • Minimized resistance and equipment stress for dynamic axial expansion
  • Comprehensive range of mountings
FEATURES:
  • ✓ Cement
  • ✓ Food & beverage
  • ✓ Forest products / Pulp & paper
  • ✓ Grain & sugar
  • ✓ Iron & steel
  • ✓ Oil & gas
  • ✓ Power generation
  • ✓ Water treatment

DISCLAIMER: The above content is provided by the supplier. Applied® does not guarantee the accuracy or timeliness of the content. 
The above content is provided “AS IS”, AND ANY AND ALL EXPRESS AND IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS ARE HEREBY EXCLUDED.
All warranties, if any, are solely from the supplier.